BRAKE#.AXIS
Description
Sets which axis will control the brake.
| Value | Description |
|---|---|
| 0 | Not used |
| 1 | Controlled by Axis 1. |
| 2 | Controlled by Axis 2. |
Examples
Context
For more information see Brake.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0 to 2 |
|
Default Value |
Depends on Brake and Axis number: BRAKE1 defaults to 1. BRAKE2 defaults to 2 on multi-axis drives and 0 on single-axis drives. |
|
Data Type |
Integer |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
|
Copyright © 2018 Kollmorgen |
|